EGEAR.LOCK
Description
EGEAR.LOCK indicates when the slave axis (follower axis) in an electronic gearing application has achieved velocity synchronization with the electronic gearing master. EGEAR.ERROR contains the amount of position deviation accumulated while the slave axis was limiting its acceleration or deceleration.
The slave axis’ acceleration or deceleration is limited to EGEAR.ACCLIMIT or EGEAR.DECLIMIT whenever:
- Gearing is turned on or turned off.
- Ratio is changed.
- EGEAR.PULSESINor EGEAR.PULSESOUT is changed.
Example
EGEAR.ACCLIMIT = 10000 EGEAR.PULSESIN = 1 EGEAR.PULSESOUT = 1 EGEAR.ERROR = 0 EGEAR.TYPE = 0 EGEAR.ON = 1 While EGEAR.LOCK = 0 : wend MOVE.RELATIVEDIST = EGEAR.ERROR MOVE.GOREL 'catch up the position lost while acceleration was being limited
General Information
|
Type |
R/O |
|
Units |
None |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1066 |
No | 8 bit | No |
M_01-05-11-000 |
Related Topics